How are the gpio arrays used in the Device Tree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How are the gpio arrays used in the Device Tree

1,984 Views
michaelworster
Contributor IV

Specifically I'm looking at the imx6qdl-sabresd.dtsi file and the ecspi1 node, below is the relevant snippet:

&ecspi1 {
    fsl,spi-num-chipselects = <1>;
    cs-gpios = <&gpio4 9 0>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_ecspi1>;

This node uses a property "cs-gpios" which is saying we're using GPIO4 with Mux option IO09 as a Chip Select for ECSPI1. However when we examine the pinctrl_ecspi1 node:

pinctrl_ecspi1: ecspi1grp {
    fsl,pins = <
        MX6QDL_PAD_KEY_COL1__ECSPI1_MISO    0x100b1
        MX6QDL_PAD_KEY_ROW0__ECSPI1_MOSI    0x100b1
        MX6QDL_PAD_KEY_COL0__ECSPI1_SCLK    0x100b1
    >;
};

There is no MX6QDL_PAD_KEY_ROW1__GPIO4_IO09 setup. From the SABRE schematics we can see "KEY_ROW1__CSPI1_CS0" is being used, which implies the pin group should have had MX6QDL_PAD_KEY_ROW1__ECSPI1_SS0 should have been configured and cs-gpios shouldn't have been used at all, but that's not the case either.

So my questions:

1) Is the pinctrl_ecspi1 group incorrect? (missing the Chip Select pin configuration) or is that done somewhere else?

2) Is chip select done by mux option ECSPI1_SS0 (as shown in the schematics) or is it done by GPIO4 (as implied by the use of cs-gpios)?

3) If chip select for ECSPI1 is via ECSPI1_SS0 is it correct to remove the cs-gpios property from this node?

Labels (3)
0 Kudos
Reply
1 Reply

1,548 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Michael.

The Device Tree is configuring that pin as GPIO because it is handled manually. if you want to configure the pin to be handled automatically by the SPI module you need to make so modications. So, regarding to your question.}

1) No, it is not wrong, the configuration is set to handle Chip Select manually.

2) Is by GPIO 4

3) To set the Chip Select for automatic functionality

   a) change fsl,spi-num-chipselects to 0. E.g. fsl,spi-num-chipselects = <0>;

   b) remove line cs-gpios = <&gpio4 9 0>;

   c) Add MX6QDL_PAD_KEY_ROW1__ECSPI1_SS0 in pinctrl_ecspi1: ecspi1grp

Hope this helps,


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply