How To Rotate 180 Degree Video For Display In I.MX8X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To Rotate 180 Degree Video For Display In I.MX8X

Jump to solution
3,390 Views
jran
Contributor II

Hello, We have designed a i.MX8QXP based product with an LVDS display.

Due to mechanical constraints, we had to mount the display upside down. Now we want to rotate the screen 180 degrees in software.

We have found that weston can do display rotation. But that doesn't include the terminal, boot logo etc.
Rotation via /sys/class/graphics/fb0/rotate seems to do nothing.

How would one go about to rotate the display?

 

I found the following thread regarding basically the same thing: https://community.nxp.com/t5/i-MX-Processors/How-To-Rotate-90-Degree-Video-For-Display-In-I-MX8X/m-p...
But the patch sent out in that thread doesn't seem to be available.

0 Kudos
Reply
1 Solution
3,380 Views
igorpadykov
NXP Employee
NXP Employee

Hi jran

 

patch was sent via mail.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
3,381 Views
igorpadykov
NXP Employee
NXP Employee

Hi jran

 

patch was sent via mail.

 

Best regards
igor

0 Kudos
Reply
2,494 Views
hf-fujita
Contributor I

Hello, 

Now I faced the same issue (need rotation, for i.MX8DXL)
Can I also get the patch ? 

 

thanks in advance & best regards, 

Hirofumi Fujita

0 Kudos
Reply
3,342 Views
aber
Contributor III

Hi  igorpadykov, jran

    I also encountered a similar problem, can I send a patch to my mailbox? Or share it, thanks

0 Kudos
Reply