Hi, could you please provide the Differential Input Voltage value VID (min, max) and Differential Output Voltage value VOD (min, max) for MCIMX6Q6AVT10AD processor for HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, could you please provide the Differential Input Voltage value VID (min, max) and Differential Output Voltage value VOD (min, max) for MCIMX6Q6AVT10AD processor for HDMI

934 Views
muralikrishna
Contributor I

Hi,

           could you please provide the Differential Input Voltage value VID (min, max) and Differential Output Voltage value VOD (min, max) for MCIMX6Q6AVT10AD processor for HDMI & DDR3L interfaces.

Labels (1)
0 Kudos
Reply
1 Reply

851 Views
igorpadykov
NXP Employee
NXP Employee

Hi Murali

i.MX6 has not HDMI input, so input HDMI characteristics are not specified.

As for output: VSWING= 400(min.) - 600(max.)  mV as given in

Figure 57 Driver Definitions, Table 63 Electrical Characteristics IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply