Hi, Could you please provide the Differential Input Voltage value VID(min, max) and Differential Output Voltage value VOD(min, max) for DDR3L interface ASAP.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, Could you please provide the Differential Input Voltage value VID(min, max) and Differential Output Voltage value VOD(min, max) for DDR3L interface ASAP.

1,024件の閲覧回数
muralikrishna
Contributor I

Hi,

Could you please provide the Differential Input Voltage value VID(min, max) and Differential Output Voltage value VOD(min, max) for DDR3L interface ASAP.

0 件の賞賛
返信
1 返信

933件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Murali

differential input voltage   0.35V (min.)  - OVDD (max.)  [Table 30]

differential output voltage   0.6*OVDD (min.)  - OVDD (max.)  [Table 24]

if keeping Voh (min.) = 0.8*OVDD and Vol (max.) = 0.2*OVDD

this could be calculated with IMX6DQCEC

Table 24. DDR3/DDR3L I/O DC Electrical Parameters

Table 30. DDR I/O DDR3/DDR3L Mode AC Parameters

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信