Hi Everyone,
I need a help to reconfigure pins of i.MX6 of Wandboard.
In Wandboard Solo and linux ubuntu downloaded from wandboard site the pins E24 and E25 are configured as GPIO6_31 and GPIO3_27, but I need to use these pins as UART2_TX and UART2_RX.
How do I do this?
I need to re-compile the kernel but what files I need to change? What parameters?
Thanks,
Gabriel