Hi,I'm looking into adding a frequency for 1280X800, and pixel clock is 83500000 Hz. would you help generate the parameters for us.
thanks.
Johnny
Hi @JohnnyDi2030,
I hope you are doing well.Please check whether the external display is supporting the resolution or not.Please check whether the resolution, one is trying to add is supported by evk or not.
If not then one has to change the clocks as per the display requirement.One can refer to the below link for reference.https://community.nxp.com/t5/i-MX-Processors/HDMI-DRM-custom-resolution-and-clock-frequency/m-p/1029...->Pixel clock - pix_clk = This clock should be configured according to TFT panel specification.
Thanks & Regards,Dhruvit Vasavada