Help generate new parameters for HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help generate new parameters for HDMI

930 Views
JohnnyDi2030
Contributor I

Hi,
I'm looking into adding a frequency for 1280X800, and pixel clock is 83500000 Hz. would you help generate the parameters for us.

thanks.

Johnny

0 Kudos
Reply
1 Reply

917 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @JohnnyDi2030,

I hope you are doing well.

Please check whether the external display is supporting the resolution or not.
Please check whether the resolution, one is trying to add is supported by evk or not.

If not then one has to change the clocks as per the display requirement.
One can refer to the below link for reference.
https://community.nxp.com/t5/i-MX-Processors/HDMI-DRM-custom-resolution-and-clock-frequency/m-p/1029...

->Pixel clock - pix_clk = This clock should be configured according to TFT panel specification.

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply