HDMI input on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI input on iMX6

2,625 Views
sadatanvashisth
Contributor I

We have a requirement of HDMI input on our system , I want to choose between interfacing either HDMI to parallel or HDMI to MIPI converter chip to iMX6. Can any one suggest that which approach is better in term of complexity , cost, availability of Linux driver and hardware implementation?

Labels (5)
0 Kudos
Reply
1 Reply

1,897 Views
gary_bisson
Senior Contributor III

Hi,

We offer such solution HDMI to MIPI:

i.MX6 HDMI Input Daughter Board 

This board is just an evaluation one, but it can be easily integrated inside a custom board design. The Linux driver is already up and running.

Feel free to reach out to our sales team for more info:

[email protected]

Regards,

Gary