HDMI Interlaced Mode Timing Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI Interlaced Mode Timing Issue

Jump to solution
2,193 Views
jonchaps
Contributor II

Hello,


The patches published at Patch for iMX6 BSP to support interlaced display on HDMI and LCD interface, which added support for HDMI interlaced modes on the iMX6, do not adhere to the timing requirements specified in the CEA-861 specification.


After applying the new version of "patch4" from the thread specified above, there is a timing issue where the VSYNC signal is offset by one pixel clock from where it should be. The CEA-861 specification states that the VSYNC should be perfectly aligned with the HSYNC signal plus or minus zero pixel clocks for field 1. For field 2 the VSYNC should be Htotal/2 pixel clocks from the leading edge of the HSYNC signal plus or minus zero pixel clocks. In both cases the VSYNC is 1 pixel clock too late. Is there a way to correct this offset on the IPU so that this functions according to the CEA spec?


I raised this issue in the original thread (HDMI Interlaced Modes), but that thread no longer appears to be active.


Thank you,

Jon

Labels (1)
0 Kudos
Reply
1 Solution
1,841 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
1 Reply
1,842 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply