H.264 Encoder + Decoder performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

H.264 Encoder + Decoder performance

3,922 Views
duduakler
Contributor I

Does the iMX6 supports 1080p@30fps encoding and decoding simultaneously?

Labels (2)
0 Kudos
Reply
4 Replies

2,464 Views
saurabh206
Senior Contributor III

Hi,

Which BSP are you using?

From specification it is possible to do.

0 Kudos
Reply

2,464 Views
duduakler
Contributor I

Hi,

Not yet using.

It is one of my system requirements and I could not find it explicitly.

Can you direct me to the document?

Thanks

0 Kudos
Reply

2,464 Views
saurabh206
Senior Contributor III

Hi,

Check following document for the VPU performance detail.

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

Thanks,

Saurabh

0 Kudos
Reply

2,464 Views
duduakler
Contributor I

Hi Saurabh,

Great Info.

Thanks,

Dudu

0 Kudos
Reply