Gstreamer1.0 plugins without X11/Wayland (dizzy )

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gstreamer1.0 plugins without X11/Wayland (dizzy )

ソリューションへジャンプ
2,843件の閲覧回数
caiopereira
Contributor III
Hello,

It's possible to compile the gstreamer1.0-plugins (base/good/bad) without X11/Wayland?
I saw that there's a dependency of gdk-pixbuf that depends x11.

I would like to use only QT5.4 with eglfs without windows manager and to decode videos (h264, RTP ).

The libx11-diet could supply this dependency?


Thank you very much.

Regards,

ラベル(7)
0 件の賞賛
返信
1 解決策
2,496件の閲覧回数
caiopereira
Contributor III

Thanks!

I already use DISTRO_remove = " x11"

But the gstreamer-plugins-good include as a default dependency with gdk-pixbuf virtua/x11.

To solve this question is needed.

PACKAGECONFIG_remove_pn-gstreamer1.0-plugins-good = " gdk-pixbuf "

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,496件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yocto can build different image, you can choose the image which doesn't include x11, for more detailed information, pls refer to the Yocto User Guide.

0 件の賞賛
返信
2,497件の閲覧回数
caiopereira
Contributor III

Thanks!

I already use DISTRO_remove = " x11"

But the gstreamer-plugins-good include as a default dependency with gdk-pixbuf virtua/x11.

To solve this question is needed.

PACKAGECONFIG_remove_pn-gstreamer1.0-plugins-good = " gdk-pixbuf "

Regards,

0 件の賞賛
返信