Gstreamer questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gstreamer questions

Jump to solution
2,428 Views
nmak
Contributor I

I'm using an IMX6Q 3.10.17.0 BSP.

Can freescale's Gstreamer 1.0 be ported to the 3.10.17 Kernel BSP?

My Gstreamer 0.10 doesn't have a videorate plugin. Is my base install broken?

Some of the element properties from tvsrc (ex. fps-n, do-timestamp do not work. Is my base install broken?)

Tags (2)
0 Kudos
Reply
1 Solution
2,108 Views
igorpadykov
NXP Employee
NXP Employee

HI Nathan

recommended to use latest BSP, it supports Gstreamer 1.0:

L3.14.28_1.0.0_iMX6QDLS_BUNDLE :

FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,

one can refer to attached file, regarding porting suggest to look at

Problems building i.MX6 image for LinuxFB with Dizzy BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,109 Views
igorpadykov
NXP Employee
NXP Employee

HI Nathan

recommended to use latest BSP, it supports Gstreamer 1.0:

L3.14.28_1.0.0_iMX6QDLS_BUNDLE :

FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,

one can refer to attached file, regarding porting suggest to look at

Problems building i.MX6 image for LinuxFB with Dizzy BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,108 Views
nmak
Contributor I

I wish I could update the BST. Unfortunately we're well into development and running the update treadmill isn't appealing to us. Can you speak to any of my questions directly?

0 Kudos
Reply