Gstreamer questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,767件の閲覧回数
nmak
Contributor I

I'm using an IMX6Q 3.10.17.0 BSP.

Can freescale's Gstreamer 1.0 be ported to the 3.10.17 Kernel BSP?

My Gstreamer 0.10 doesn't have a videorate plugin. Is my base install broken?

Some of the element properties from tvsrc (ex. fps-n, do-timestamp do not work. Is my base install broken?)

タグ(2)
0 件の賞賛
返信
1 解決策
3,445件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Nathan

recommended to use latest BSP, it supports Gstreamer 1.0:

L3.14.28_1.0.0_iMX6QDLS_BUNDLE :

FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,

one can refer to attached file, regarding porting suggest to look at

Problems building i.MX6 image for LinuxFB with Dizzy BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,446件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Nathan

recommended to use latest BSP, it supports Gstreamer 1.0:

L3.14.28_1.0.0_iMX6QDLS_BUNDLE :

FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,

one can refer to attached file, regarding porting suggest to look at

Problems building i.MX6 image for LinuxFB with Dizzy BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,445件の閲覧回数
nmak
Contributor I

I wish I could update the BST. Unfortunately we're well into development and running the update treadmill isn't appealing to us. Can you speak to any of my questions directly?

0 件の賞賛
返信