Gstreamer questions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Gstreamer questions

跳至解决方案
3,766 次查看
nmak
Contributor I

I'm using an IMX6Q 3.10.17.0 BSP.

Can freescale's Gstreamer 1.0 be ported to the 3.10.17 Kernel BSP?

My Gstreamer 0.10 doesn't have a videorate plugin. Is my base install broken?

Some of the element properties from tvsrc (ex. fps-n, do-timestamp do not work. Is my base install broken?)

标记 (2)
0 项奖励
回复
1 解答
3,444 次查看
igorpadykov
NXP Employee
NXP Employee

HI Nathan

recommended to use latest BSP, it supports Gstreamer 1.0:

L3.14.28_1.0.0_iMX6QDLS_BUNDLE :

FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,

one can refer to attached file, regarding porting suggest to look at

Problems building i.MX6 image for LinuxFB with Dizzy BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,445 次查看
igorpadykov
NXP Employee
NXP Employee

HI Nathan

recommended to use latest BSP, it supports Gstreamer 1.0:

L3.14.28_1.0.0_iMX6QDLS_BUNDLE :

FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,

one can refer to attached file, regarding porting suggest to look at

Problems building i.MX6 image for LinuxFB with Dizzy BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,444 次查看
nmak
Contributor I

I wish I could update the BST. Unfortunately we're well into development and running the update treadmill isn't appealing to us. Can you speak to any of my questions directly?

0 项奖励
回复