I'm using an IMX6Q 3.10.17.0 BSP.
Can freescale's Gstreamer 1.0 be ported to the 3.10.17 Kernel BSP?
My Gstreamer 0.10 doesn't have a videorate plugin. Is my base install broken?
Some of the element properties from tvsrc (ex. fps-n, do-timestamp do not work. Is my base install broken?)
已解决! 转到解答。
HI Nathan
recommended to use latest BSP, it supports Gstreamer 1.0:
L3.14.28_1.0.0_iMX6QDLS_BUNDLE :
FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,
one can refer to attached file, regarding porting suggest to look at
Problems building i.MX6 image for LinuxFB with Dizzy BSP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Nathan
recommended to use latest BSP, it supports Gstreamer 1.0:
L3.14.28_1.0.0_iMX6QDLS_BUNDLE :
FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,
one can refer to attached file, regarding porting suggest to look at
Problems building i.MX6 image for LinuxFB with Dizzy BSP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------