GPS Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPS Problem

3,009 Views
rambabugedela
Contributor I

hi ,

i am using AH-1613 GPS Module in our Project.I am interfacing gps module to imx6dl through UART2 . I have problem is that i am not able to get output Nmea message. please help me how to get output Nmea messages

Regard

G.Rambabu

Labels (4)
0 Kudos
Reply
3 Replies

2,449 Views
napster_k
Contributor II

Sometimes you need to set the gps speed before reading the nmea msgs

0 Kudos
Reply

2,790 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,790 Views
rambabugedela
Contributor I

hi;

Thanks for your Reply.

I am using VAR-SOM-MX6 android build for our custom imx6 board but in

VAR-SOM-MX6 android build there is no supported to AH-1613 gps module.

I am using ttymxc2 for gps. Here problem is that gps app not working and

I add my log messages also

root@var_som_mx6:/dev # ls -l

-rrr-- root root 131072 1970-01-01 00:00 __properties__

crw-rw-r-- system radio 10, 52 1970-01-01 00:00 alarm

crw-rw---- adb adb 10, 56 1970-01-01 00:00 android_adb

crw

0 Kudos
Reply