GPMI NAND Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPMI NAND Mode

Jump to solution
2,407 Views
takashitakahash
Contributor III

Dear community.

i.MX6DQ RM of 29.4 GPMI NAND Mode Describes on Check Status-The Read-and-Compare mode allows the GPMI to check NAND status against a reference.

What check is this?
Will check the verify the written data ?

Labels (2)
0 Kudos
Reply
1 Solution
2,212 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

this command compares read data (usually NAND status)

with REFERENCE data as described in

IMX6DQRM 29.6.2 GPMI Compare Register Description (GPMI_COMPARE)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,213 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

this command compares read data (usually NAND status)

with REFERENCE data as described in

IMX6DQRM 29.6.2 GPMI Compare Register Description (GPMI_COMPARE)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply