GPIO configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO configuration

Jump to solution
2,022 Views
adde_ado
Contributor III

Hi,

I'm using a GPIO (input) to read data from an IC circuit. 

Output pin on IC that I'm trying to read is an open drain output with internal pull-up resistor. 

I'm wondering how I should configure my GPIO input pin.

IOMUXC_SetPinMux(IOMUXC_SAI3_RXFS_GPIO4_IO28, 0U);

IOMUXC_SetPinConfig(IOMUXC_SAI3_RXFS_GPIO4_IO28, 0x??);

Best regards,

Ado

 

Labels (1)
0 Kudos
Reply
1 Solution
1,993 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adnan

 

for these settings one can look at sect.8.2 IOMUX Controller (IOMUXC)

i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

sect.8.2.5.111 SW_MUX_CTL_PAD_SAI3_RXFS SW MUX Control Register
(IOMUXC_SW_MUX_CTL_PAD_SAI3_RXFS), sect.8.2.5.265 SW_PAD_CTL_PAD_SAI3_RXFS

SW PAD Control Register (IOMUXC_SW_PAD_CTL_PAD_SAI3_RXFS)

 

Best regards
igor

View solution in original post

1 Reply
1,994 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adnan

 

for these settings one can look at sect.8.2 IOMUX Controller (IOMUXC)

i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

sect.8.2.5.111 SW_MUX_CTL_PAD_SAI3_RXFS SW MUX Control Register
(IOMUXC_SW_MUX_CTL_PAD_SAI3_RXFS), sect.8.2.5.265 SW_PAD_CTL_PAD_SAI3_RXFS

SW PAD Control Register (IOMUXC_SW_PAD_CTL_PAD_SAI3_RXFS)

 

Best regards
igor