G2D plugins don't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

G2D plugins don't work

ソリューションへジャンプ
2,744件の閲覧回数
pierre-olivierh
Contributor III

Hello,

I'm trying to make G2D plugins from gstreamer-imx work with my imx6q. I work on Yocto, fido branch, with 3.14.38 kernel.

These plugins are from https://github.com/Freescale/gstreamer-imx. When I try to run gst-launch-1.0 imxv4l2videosrc ! imxg2dvideosink I get the following error :

g2d_alloc: alloc memory fail with size 16!
ERROR: Pipeline doesn't want to pause.
Setting pipeline to NULL ...
Freeing pipeline ..

With more debug :

0:00:00.540714000   425   0x549400 INFO     imxphysmemallocator phys_mem_allocator.c:62:gst_imx_phys_mem_allocator_init:<GstImxPhysMemAllocator@0x54d908> initializing physical memory allocator
g2d_alloc: alloc memory fail with size 16!
0:00:00.556959667   425   0x549400 ERROR        imxg2dallocator allocator.c:59:gst_imx_g2d_alloc_phys_mem:<imxg2dallocator0> could not allocate 16 bytes of physical memory
0:00:00.557108000   425   0x549400 WARN     imxphysmemallocator phys_mem_allocator.c:154:gst_imx_phys_mem_allocator_alloc:<imxg2dallocator0> could not allocate memory block with 16 bytes
0:00:00.557213000   425   0x549400 WARN              GST_BUFFER gstbuffer.c:739:gst_buffer_new_allocate: failed to allocate 16 bytes

I posted an issue on the github, but it's not solved.

I tried to change the CMA value, already to 320M to other values, but this the same error.

a part of my kernel configuration :

CONFIG_MXC_GPU_VIV=y

CONFIG_CMA_SIZE_MBYTES=320
CONFIG_CMA_SIZE_SEL_MBYTES=y

CONFIG_CMA_ALIGNMENT=8
CONFIG_CMA_AREAS=7

CONFIG_DMA_CMA=y

CONFIG_DMA_SHARED_BUFFER=y

I think it would be a kernel missconfiguration. I work on another iMX (DL) and these plugins just work fine with yocto fido. Any thougts about kernel missing configuration?

Best Regards

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,185件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pierre

please refer to below link about gstreamer-imx support

Gstreamer imxvpuap error 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,186件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pierre

please refer to below link about gstreamer-imx support

Gstreamer imxvpuap error 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信