I need to use network stack on my project, but due to some reasons similar to one listed as below link
Using NonCached Memory on i.MXRT - NXP Community
Even after following the solution listed, we are facing similar issues
Can you help me in following
1. FreeRTOS has its own TCP/IP stack
2. Need some demo example which can help me to run Frtos with tcp on USB-RNDIS interface
I was able to get lwip+frtos, but i need frtos+tcp example
Kindly suggest
Hi @shrinivasnh
I understand that you are willing to implement FreeRTOS open source TCP/IP stack instead of LWIP stack, as our lwip_dhcp_usb SDK examples do. Is this correct? If yes:
Available information that I know it may help is in the FreeRTOS documentation ( link from above) and from our AN13940 Connect i.MX RT1060 to USB 4G Module (RNDIS Mode)
Regarding the link you shared Using NonCached Memory on i.MXRT - NXP Community and the issues you mention to face. Are they related to MPU settings? Are the issues the reason why you are looking for a different stack for TCP/IP?
Please kindly correct me if needed and if you got more details on your application let me know.
All the best,
Diego