FlexCAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexCAN

1,778 次查看
nuttakorntrirat
Contributor II

I need to use CAN 2.0A and 2.0B to communicate the external device.

But, IMX6UL is FIexCAN type. Can the FlexCAN supports CAN 2.0A and 2.0B?

If it does not support, Could you please recommend me what adding external IC?

标签 (1)
标记 (1)
2 回复数

1,624 次查看
art
NXP Employee
NXP Employee

FlexCAN is just the name for the CAN controller IP of the i.MX6 series processors, and, yes, it supports both CAN 2.0 Part A and CAN 2.0 Part B specifications.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,624 次查看
nuttakorntrirat
Contributor II

Hi Petukhov, 

                   Mang thanks for your answer.

Nuttakorn

0 项奖励
回复