FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN

1,779件の閲覧回数
nuttakorntrirat
Contributor II

I need to use CAN 2.0A and 2.0B to communicate the external device.

But, IMX6UL is FIexCAN type. Can the FlexCAN supports CAN 2.0A and 2.0B?

If it does not support, Could you please recommend me what adding external IC?

ラベル(1)
タグ(1)
2 返答(返信)

1,625件の閲覧回数
art
NXP Employee
NXP Employee

FlexCAN is just the name for the CAN controller IP of the i.MX6 series processors, and, yes, it supports both CAN 2.0 Part A and CAN 2.0 Part B specifications.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,625件の閲覧回数
nuttakorntrirat
Contributor II

Hi Petukhov, 

                   Mang thanks for your answer.

Nuttakorn

0 件の賞賛
返信