igorpadykov
Dear Igor-san,
We checked about these GPIOs in LPSR mode.
NVCC_GPIO1 and NVCC_GPIO2 are supplied power to by VDD_LPSR(1.8V).
In LPSR mode,
GPIO1_IO00-GPIO1_IO07 can hold output High.
However, GPIO1_IO08-GPIO1_IO15 can not hold output High.(The output voltage drops to Low.)
Is there any necessary setting?
GPIO1_IO08-GPIO1_IO15 can be worked normally in LPSR mode?
When it is in RUN mode, GPIO1_IO08-GPIO1_IO15 works normally.
And I understand that GPIO1_IO08-GPIO1_IO15 can be used as wake-up source.
May I have advice?
Best Regards,
Yuuki