FlexCAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCAN

1,772 Views
nuttakorntrirat
Contributor II

I need to use CAN 2.0A and 2.0B to communicate the external device.

But, IMX6UL is FIexCAN type. Can the FlexCAN supports CAN 2.0A and 2.0B?

If it does not support, Could you please recommend me what adding external IC?

Labels (1)
Tags (1)
2 Replies

1,618 Views
art
NXP Employee
NXP Employee

FlexCAN is just the name for the CAN controller IP of the i.MX6 series processors, and, yes, it supports both CAN 2.0 Part A and CAN 2.0 Part B specifications.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,618 Views
nuttakorntrirat
Contributor II

Hi Petukhov, 

                   Mang thanks for your answer.

Nuttakorn

0 Kudos
Reply