FSL gnome release package and VGA display output ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FSL gnome release package and VGA display output ?

18,651 次查看
philippecavenel
Contributor I
Hello,

I can't get  a VGA output display with ltib (FSL gnome release package ). I am looking for a solution, but at that time I don't know how to proceed. I already started some discussion on that topic in this forum, but perhaps the group "graphics & display"  may have the solution !

With standard UBUNTU distribution image, my VGA display works fine (I only have a VGA display connected to the VGA output, I don't use LCD touch screen).

With ltib, nothing happens ! no image, no signal, nothing...

Last boot trace can be found in attachment.

Many thanks in advance for your help.

Best Regards,

Philippe.


标签 (1)
标记 (2)
0 项奖励
回复
22 回复数

17,894 次查看
philippecavenel
Contributor I

Congratulations ! effectively, I tried to replace my Apple keyboard by a Dell keyboard and I replaced in startx script

Xfbdev -keybd keyboard,,device=/dev/input/keyboard0 by

Xfbdev -keybd keyboard,,device=/dev/input/event2

And It works fine now.

Thank you for your support.

Regards,

Philippe.

0 项奖励
回复

17,894 次查看
hake
NXP Employee
NXP Employee

rwxrwxrwx    1 root     root             9 Jan  1 00:00 usb-Logitech_USB-PS.2_Optical_Mouse-event-mouse -> ../event4

is this a mouse or keyboard? which conflicts with your former log

usb 2-1: new high speed USB device using fsl-ehci and address 4
usb 2-1: New USB device found, idVendor=05ac, idProduct=1006
usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
usb 2-1: Product: Keyboard Hub
usb 2-1: Manufacturer: Apple, Inc.
usb 2-1: SerialNumber: 000000000000
hub 2-1:1.0: USB hub found
hub 2-1:1.0: 3 ports detected
usb 2-1.2: new low speed USB device using fsl-ehci and address 5
usb 2-1.2: New USB device found, idVendor=05ac, idProduct=0221
usb 2-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 2-1.2: Product: Apple Keyboard
usb 2-1.2: Manufacturer: Apple, Inc

0 项奖励
回复

17,894 次查看
hake
NXP Employee
NXP Employee

no you ls result shows that the usb keyboard does not recognized by the system, can you change another usb key board?

0 项奖励
回复

17,894 次查看
philippecavenel
Contributor I

Hello,

 

I selected udev and 'include automount rules' in ltib configuration. Keyboard should be automatically recognized, and it's not the case as far as I can see in /dev/input :

 

root@freescale /dev/input$ ls -lR
.:
drwxr-xr-x    2 root     root            80 Jan  1 00:00 by-id
drwxr-xr-x    2 root     root           120 Jan  1 00:00 by-path
crw-r-----    1 root     root       13,  64 Jan  1 00:00 event0
crw-r-----    1 root     root       13,  65 Jan  1 00:00 event1
crw-r-----    1 root     root       13,  66 Jan  1 00:00 event2

crw-r-----    1 root     root       13,  67 Jan  1 00:00 event3
crw-r-----    1 root     root       13,  68 Jan  1 00:00 event4
crw-r-----    1 root     root       13,  63 Jan  1 00:00 mice
crw-r-----    1 root     root       13,  32 Jan  1 00:00 mouse0
crw-r-----    1 root     root       13,  33 Jan  1 00:00 mouse1
crw-------    1 root     root       10, 223 Jan  1 00:00 uinput

./by-id:
lrwxrwxrwx    1 root     root             9 Jan  1 00:00 usb-Logitech_USB-PS.2_Optical_Mouse-event-mouse -> ../event4

lrwxrwxrwx    1 root     root             9 Jan  1 00:00 usb-Logitech_USB-PS.2_Optical_Mouse-mouse -> ../mouse1

./by-path:
lrwxrwxrwx    1 root     root             9 Jan  1 00:00 platform-da9052-onkey-event- -> ../event2
lrwxrwxrwx    1 root     root             9 Jan  1 00:00 platform-fsl-ehci.0-usb-0:1:1.0-event-mouse -> ../event4
lrwxrwxrwx    1 root     root             9 Jan  1 00:00 platform-fsl-ehci.0-usb-0:1:1.0-mouse -> ../mouse1
lrwxrwxrwx    1 root     root             9 Jan  1 00:00 platform-gpio-keys-event- -> ../event0

 

I tried mdev but it failed. I also took a look into bin/device_table.txt and keyboard is not defined. So I am wondering if I have to add it in this file or if the setting should be done somewhere else.

 

Regards,

Philippe.

0 项奖励
回复

17,894 次查看
hake
NXP Employee
NXP Employee

the keyboard and mouse are input devices, so you need check it at /dev/input/

0 项奖励
回复

17,894 次查看
philippecavenel
Contributor I

Hello hake,

 

I don't know in fact as /dev/keyboard0 is not present. when I plug in the keyboard I get :

usb 2-1: new high speed USB device using fsl-ehci and address 4
usb 2-1: New USB device found, idVendor=05ac, idProduct=1006
usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
usb 2-1: Product: Keyboard Hub
usb 2-1: Manufacturer: Apple, Inc.
usb 2-1: SerialNumber: 000000000000
hub 2-1:1.0: USB hub found
hub 2-1:1.0: 3 ports detected
usb 2-1.2: new low speed USB device using fsl-ehci and address 5
usb 2-1.2: New USB device found, idVendor=05ac, idProduct=0221
usb 2-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 2-1.2: Product: Apple Keyboard
usb 2-1.2: Manufacturer: Apple, Inc

On device, each time I unplug / plug my keyboard, I get two new devices :

crw-rw----    1 root     root      189, 135 Jan  1 00:43 /dev/usbdev2.8
crw-rw----    1 root     root      189, 136 Jan  1 00:43 /dev/usbdev2.9

(8 and 9 are incremented at each unplug / plug action,  next values  are 10 and 11 and so on).

I tried to use some other keyboards, but the result is the same, nothing happens when I press on keys. My aim is to recognize all kind of keyboards as I have no idea of what kind of keyboard people will use on my application.


I don't use touch screen, just a VGA display + mouse + keyboard + serial interface to configure the system.

 

Regards,

Philippe.

0 项奖励
回复

17,894 次查看
hake
NXP Employee
NXP Employee

what is your keypad input device node? you can use evtest /dev/input/<your device node> to test, then set to the device parameter. No sure it is going to work or not, as the key definitions may need change, you have to look at the xfb code.

0 项奖励
回复

17,894 次查看
philippecavenel
Contributor I

OK for the SD card, effectively I specify BS=512.

Concerning the keyboard I updated startx script with -keybd keyboard,,device=/dev/input/keyboard0 but in fact there is no keyboard0 in /dev/input, so it can't work. Do you know how to configure keyboard device ? Is it a special configuration in ltib ?

0 项奖励
回复

17,894 次查看
hake
NXP Employee
NXP Employee

there are some configs for keyboard support, you can check that in startx scripts.

if skip=1 seek=1 does not work, which mean your SD card can only seek in 512 bytes block.

0 项奖励
回复

17,894 次查看
philippecavenel
Contributor I

Hello,

Thank you for your help.

After a while, with the last release 11.09 I finally got an output on my VGA display. Now, the mouse is working fine on my X window environment but my keyboard is not recognized, nothing happens when I press on keys....

 

Do you know if there is a specific configuration for the startx script ? especially for Xfbdev ?

 

By the way, dd if=<uboot> of=/dev/mmcblk0 bs=1024 seek=1 skip=1 doesn't work for me, I have to specify seek=2 skip=2.

 

Best Regards,

Philippe.

0 项奖励
回复

17,895 次查看
hake
NXP Employee
NXP Employee
dd if=<uboot> of=/dev/mmcblk0 bs=1024 seek=1 skip=1
0 项奖励
回复

17,895 次查看
philippecavenel
Contributor I
It doesn't boot... which dd command do you use ?
0 项奖励
回复

17,894 次查看
hake
NXP Employee
NXP Employee
in this case you need uboot
0 项奖励
回复

17,893 次查看
philippecavenel
Contributor I

I tried to replace my uImage by your uImage_mx53_d but it failed. (see trace.txt).

 

Regards,

Philippe.

0 项奖励
回复

17,893 次查看
hake
NXP Employee
NXP Employee
can you try attached image, the "video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga" works for my board.
0 项奖励
回复

17,893 次查看
philippecavenel
Contributor I

Hello hake,

root@freescale ~$ cat /proc/cmdline
console=ttymxc0,115200 video=mxcdi1fb:GBR24,XGA di1_primary vga root=/dev/mmcblk0p1 rw rootwait

 

Regards,

Philippe

0 项奖励
回复

17,893 次查看
hake
NXP Employee
NXP Employee

cat you boot board and

cat /proc/cmdline to judge the command line also.

the 1105 release should be work

0 项奖励
回复

17,893 次查看
philippecavenel
Contributor I
Al,


Yes, on UBUNTU distribution I have :

vga=video=mxcdi1fb:GBR24,XGA di1_primary tve

bootargs_base=setenv bootargs console=ttymxc0,115200 ${vga}


I tried this setting, but no more result.


Where did you specify in ltib setting that you use videos/imxfb driver ?


Regards,

Philippe.


0 项奖励
回复

17,893 次查看
AlHauer
Contributor I

Philippe,

I assume you already halted your Ubuntu distribution image at u-boot console, and viewed the environment variables, where "video=" would be found?  If so, what were the options to the kernel?  I am using the videos/imxfb driver.

-Al

0 项奖励
回复

17,892 次查看
philippecavenel
Contributor I

Hello Al & Hake,

 

thank you for answering. I tried to add video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga ldb=off ard-vga but, it didn't work.

 

I tried to replace by video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga but it didn't work.

I guess the problem is more in the ltib setting. Do you know what packages and/or driver I have to use for VGA display output ?

 

(I attached my last boot log).

 

Regards,

Philippe

0 项奖励
回复