U-Boot 2009.08 (Oct 31 2011 - 19:11:45) CPU: Freescale i.MX53 family 2.0V at 1000 MHz mx53 pll1: 1000MHz mx53 pll2: 400MHz mx53 pll3: 216MHz mx53 pll4: 455MHz ipg clock : 66666666Hz ipg per clock : 33333333Hz uart clock : 21600000Hz cspi clock : 54000000Hz ahb clock : 133333333Hz axi_a clock : 400000000Hz axi_b clock : 200000000Hz emi_slow clock: 133333333Hz ddr clock : 400000000Hz esdhc1 clock : 80000000Hz esdhc2 clock : 80000000Hz esdhc3 clock : 80000000Hz esdhc4 clock : 80000000Hz nfc clock : 26666666Hz Board: MX53-LOCO 1.0 Boot Reason: [POR] Boot Device: SD I2C: ready DRAM: 1 GB MMC: FSL_ESDHC: 0, FSL_ESDHC: 1 In: serial Out: serial Err: serial Net: got MAC address from IIM: 00:04:9f:01:c9:60 FEC0 [PRIME] Hit any key to stop autoboot: 3  2  1  0 MMC read: dev # 0, block # 2048, count 6144 partition # 0 ... 6144 blocks read: OK ## Booting kernel from Legacy Image at 70800000 ... Image Name: Linux-2.6.35.3-daily-01137-g98d7 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3004972 Bytes = 2.9 MB Load Address: 70008000 Entry Point: 70008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Linux version 2.6.35.3-daily-01137-g98d71e8 (ubuntu@kvmserver) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #1 PREEMPT Thu Nov 3 22:07:25 CST 2011 CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache Machine: Freescale MX53 LOCO Board Memory policy: ECC disabled, Data cache writeback Built 1 zonelists in Zone order, mobility grouping on. Total pages: 250880 Kernel command line: console=ttymxc0,115200 video=mxcdi1fb:GBR24,XGA di1_primary vga root=/dev/mmcblk0p1 rw rootwait PID hash table entries: 4096 (order: 2, 16384 bytes) Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) Memory: 480MB 512MB = 992MB total Memory: 998236k/998236k available, 17572k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xf9e00000 - 0xffe00000 ( 96 MB) vmalloc : 0xe0800000 - 0xf4000000 ( 312 MB) lowmem : 0x80000000 - 0xe0000000 (1536 MB) pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) modules : 0x7f000000 - 0x7fe00000 ( 14 MB) .init : 0x80008000 - 0x80033000 ( 172 kB) .text : 0x80033000 - 0x807f6000 (7948 kB) .data : 0x80814000 - 0x8086c0a0 ( 353 kB) SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Hierarchical RCU implementation. RCU-based detection of stalled CPUs is disabled. Verbose stalled-CPUs detection is disabled. NR_IRQS:368 MXC GPIO hardware MXC IRQ initialized MXC_Early serial console at MMIO 0x53fbc000 (options '115200') bootconsole [ttymxc0] enabled Console: colour dummy device 80x30 Calibrating delay loop... 999.42 BogoMIPS (lpj=4997120) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok regulator: core version 0.5 NET: Registered protocol family 16 i.MX IRAM pool: 128 KB@0xe0840000 IRAM READY CPU is i.MX53 Revision 2.0 Using SDMA I.API MXC DMA API initialized IMX usb wakeup probe IMX usb wakeup probe bio: create slab at 0 SCSI subsystem initialized Freescale USB OTG Driver loaded, $Revision: 1.55 $ ****************************** NOTICE ***************************** You have seen this notice as you have enabled OTG driver for mx53 LOCO board For mx53 loco board, the OTG function is unavailable due to hardware limitation So, Only one usb function (device or host) can be available for certain image Please config your kernel to disable OTG and the usb function you don't want to use And remain the other usb function you would like to use Below OTG configs should be removed: CONFIG_MXC_OTG, CONFIG_USB_OTG Choose one of below configs for host or device function But DO NOT choose them together OTG host config CONFIG_USB_EHCI_ARC_OTG OTG device config CONFIG_USB_GADGET usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb da9052_i2c_is_connected - i2c read success.... regulator: DA9052_LDO1: 600 <--> 1800 mV at 1300 mV normal regulator: DA9052_LDO2: 600 <--> 1800 mV at 1300 mV normal regulator: DA9052_LDO3: 1725 <--> 3300 mV at 3300 mV normal regulator: DA9052_LDO4: 1725 <--> 3300 mV at 2775 mV normal regulator: DA9052_LDO5: 1200 <--> 3600 mV at 1300 mV normal regulator: DA9052_LDO6: 1200 <--> 3600 mV at 1300 mV normal regulator: DA9052_LDO7: 1200 <--> 3600 mV at 2750 mV normal regulator: DA9052_LDO8: 1200 <--> 3600 mV at 1800 mV normal regulator: DA9052_LDO9: 1250 <--> 3650 mV at 2500 mV normal regulator: DA9052_LDO10: 1200 <--> 3600 mV at 1300 mV normal regulator: DA9052_BUCK_CORE: 500 <--> 2075 mV at 1200 mV normal regulator: DA9052_BUCK_PRO: 500 <--> 2075 mV at 1300 mV normal regulator: DA9052_BUCK_MEM: 925 <--> 2500 mV at 1500 mV normal regulator: DA9052_BUCK_PERI: 1800 <--> 3600 mV at 3600 mV normal DA9053 chip ID reg read=0xa3 BB version probed IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) Advanced Linux Sound Architecture Driver Version 1.0.23. Bluetooth: Core ver 2.15 NET: Registered protocol family 31 Bluetooth: HCI device and connection manager initialized Bluetooth: HCI socket layer initialized Switching to clocksource mxc_timer1 NET: Registered protocol family 2 IP route cache hash table entries: 32768 (order: 5, 131072 bytes) TCP established hash table entries: 131072 (order: 8, 1048576 bytes) TCP bind hash table entries: 65536 (order: 6, 262144 bytes) TCP: Hash tables configured (established 131072 bind 65536) TCP reno registered UDP hash table entries: 512 (order: 1, 8192 bytes) UDP-Lite hash table entries: 512 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. LPMode driver module loaded Static Power Management for Freescale i.MX5 PM driver module loaded sdram autogating driver module loaded Bus freq driver module loaded DI1 is primary mxc_dvfs_core_probe DVFS driver module loaded i.MXC CPU frequency driver DVFS PER driver module loaded JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc. msgmni has been set to 1949 alg: No test for stdrng (krng) cryptodev: driver loaded. io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) regulator: get() with no identifier By setting, SII driver will not be enabled By setting, LDB driver will not be enabled mxc_ipu mxc_ipu: Channel already disabled 9 mxc_ipu mxc_ipu: Channel already uninitialized 9 Console: switching to colour frame buffer device 100x30 mxc_ipu mxc_ipu: Channel already disabled 7 mxc_ipu mxc_ipu: Channel already uninitialized 7 mxc_ipu mxc_ipu: Channel already disabled 10 mxc_ipu mxc_ipu: Channel already uninitialized 10 Serial: MXC Internal UART driver mxcintuart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a Freescale i.MX |g3Or Opg8SansOGt 3O 03O?!30&> >>0> &33<x 03LfN) 8<3303 &8&3630&> > >0> &3<x 03Lf~38<3302 &8&36!Ɔ&2030&> >>0> &3<x 03Lf@H(~rp !&6030&> >0>0> &3&LR.  px033sa~03 trg>00O6 0Og3&030&3Og2>& 0<08Ld`83 & >&&6`.i@@@ߑ83g&20&&3&&>>0|a~ 3g3&ga&083a\&@g3Og0"(Y03 Cda 3>& 383O`g2083O`g2eTee!r綨!؎ h@@@13{830g?)83O`g6083O`g683O`g2083O`g2??????Y@@]LM\]L83O`g6083O`g6Æ>0 &8&36!Cf`& Cdr0Og383O`g6083O`g6Æ>0Þ6?03&&308>Ϗ>& &8 H 3883O`g6083O`g6Æ>03sc~03<ai{{p83O`g2083O`g2Æ>03&&3!/dev/ttyUSB1 : 115200ؔq>6<!P\|~'z~IB}r)-H00) { 0.8667, 0.2824, 0.0784 }llorcSkt) { 0x0 , 0x0 , 0x0 , 0x0 } (Pɒ뱶h/0sd> &8&rHXXXX(Y`YYZO&> 8&0s838))Hi p?&!@#@&@ \G94dsi dʇI83O`g2083O`g2Æ03sc~03<bťn3b҇/ ,zӉ2b҇/,v%b҇/ m׍3b҇/,v&b҇/,yԋ3 bǨq5g՗el L蒕|?+ &60 >. - Hѕ2@2@??2@2@$m?$m?2@3@@7@7@ҕ`X~8ŕ`c跃q\p@&60|a~0Opghgח  /C (>0Þ6?03&&3 *FA(I08Ld`83 &sd&??Q08Ld`83 &sd&???$P(+|Oٶ|Oٶ|OٶЌH+|Oٶ茕|Oٶ`|OٶB|Oٶ0B|Oٶ`B|Oٶ%|OٶxQ|Oٶ{Oٶ`{0 &>& 33g0O p`3s~g p`82( Br@Gr@p8h0PP8Q p`f03O&88&>&&O|g&> O&> 800g????i@@@ߑ?Hd?H)kz-> Q Q!r@v(i3XV?$@$@@0>& 0<86&sp&8 68>Ϗ>& &8 ,0 i%@@@8Cgyf&ϳ38am<.eliF/>niam<.wodniWktGHPu'^iz # @@샛.0ԇ. Pj8jk(k,l lkhj\kX`kdkjxgk=kPlzl0kMkyzkk klIk l`kX4kkXpjLlxy` kXkPkjk hrx8 6 pf 03<1ߒ6{5@U4&8<1&8<|c>03&0Lf & 31 &88&8p@ 03OgQ&8 Checksum ..8001 &88&8' Lohit Ta 6695) )83&36Nnel already disabled 10 mxc_ipu mxc_ipu: Chanxc_ UDP-Lite hash table&32Ёal regu1&&8&38338 &3 L>&&3 6>88 &8 8><??88&86̘ &83 px  &&3 `fg>06?03s8)838kupOٶg99): @Y@va #)>0Þ6?03&&Ȑ d@!3882ό02Og>&0 03spy638 &3 L>&&3 6>88 &8<<h388<<@B8&86y~ эw9r } ȑ&`@8>6 Og(Ogy8<~)_NET_WM_WI8>Ϗ>& &8 s3̰& 68>Ϗ>& &8 YL |g0Og03C|8LOٶি 63̰& 68>Ϗ>& &8 9(9H)+R Og0&803Þ0&3&8 sϳ&8 0?yf?A????@Br@Gr@p8h0PP8QQhRSS0TT`UUV(WA@yx)HX&8 0?a`3̀&) { 0.8667, 0.2824, 0.0784 }llorcSkt) { 0x0 , 0x0 , 0x0 , 0x0 } (0&0݉.p@!&8r&ƞ0&p@,( 0 ????R@R@r@r@  P$  &><&83  @{&8>30&ƞ0&HSansOGte6 D X Y ?H J D UG H (@H Q  FK LH U!3rOٶ"00]XVি&8r&Br@Gr@p8h0PP8Q