External device access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External device access

1,871件の閲覧回数
kimsangyoung
Contributor I

freescale i.mx6q evb was purchased. newly created board in i.mx6q. Is there a software tool that can check an external device? For example, if the access i2c exactly ?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,772件の閲覧回数
EricNelson
Senior Contributor II

Under Linux, you can use the i2c-tools package to access an I2C bus from userspace.

0 件の賞賛
返信

1,772件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kim

one can check almost all peripherals with SDK:

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series, including reusable

drivers and tests for many peripherals, and much example code.

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信