External device access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External device access

1,958 Views
kimsangyoung
Contributor I

freescale i.mx6q evb was purchased. newly created board in i.mx6q. Is there a software tool that can check an external device? For example, if the access i2c exactly ?

Labels (2)
0 Kudos
Reply
2 Replies

1,859 Views
EricNelson
Senior Contributor II

Under Linux, you can use the i2c-tools package to access an I2C bus from userspace.

0 Kudos
Reply

1,859 Views
igorpadykov
NXP Employee
NXP Employee

Hi kim

one can check almost all peripherals with SDK:

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series, including reusable

drivers and tests for many peripherals, and much example code.

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply