Ethernet stops when WiFi connected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet stops when WiFi connected

Jump to solution
1,802 Views
himanshugusain
Contributor III

Hi we have a custom sabresd board in which freescale provided android lollipop

is running ,We have connected sabresd to  another device (running on linux )

through ethernet interface(static IP).

Now when we connect our sabresd board to WiFi network  the ethernet connection(between sabresd and other device )

doesn't works(verified by pinging )

What could be the possible reason

Regards

Himanshu

Labels (3)
0 Kudos
Reply
1 Solution
1,633 Views
BiyongSUN
NXP Employee
NXP Employee

Could you please check the routing table to find the default routing interface in that time?

View solution in original post

0 Kudos
Reply
1 Reply
1,634 Views
BiyongSUN
NXP Employee
NXP Employee

Could you please check the routing table to find the default routing interface in that time?

0 Kudos
Reply