Ethernet stops when WiFi connected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet stops when WiFi connected

ソリューションへジャンプ
1,803件の閲覧回数
himanshugusain
Contributor III

Hi we have a custom sabresd board in which freescale provided android lollipop

is running ,We have connected sabresd to  another device (running on linux )

through ethernet interface(static IP).

Now when we connect our sabresd board to WiFi network  the ethernet connection(between sabresd and other device )

doesn't works(verified by pinging )

What could be the possible reason

Regards

Himanshu

ラベル(3)
0 件の賞賛
返信
1 解決策
1,634件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

Could you please check the routing table to find the default routing interface in that time?

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,635件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

Could you please check the routing table to find the default routing interface in that time?

0 件の賞賛
返信