Ethernet compliance testing of Linux board based on iMX6UL & KSZ8041NLI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet compliance testing of Linux board based on iMX6UL & KSZ8041NLI

1,690 次查看
ghanshyamdudhat
Contributor I

Dear Sir,

We are testing our product for Ethernet compliance testing through DSO Pre-compliance test module but as per test procedure need a test firmware with predefined test packet,

refer the required format -  scrambled, MLT-3 encoded /I/ code-groups (this is a 3-level pseudo-random bit sequence).

Can any one help us to create test application or share with us the application note or test firmware (Linux operating System) to perform the mentioned test.

 

Refer the below NXP and Mirochip PHY part details –

NXP Processer: iMX6UL

Ethernet PHY : KSZ8041NLI-TR

 

 Ethernet section schematic :

 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,568 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ghanshyam 

I am afraid such ethernet compliance test application is not available, in general
one can aply to Professional Services to develop such test.
NXP Professional Services|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复