bitbake fsl-image-qt5 failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake fsl-image-qt5 failed

3,009 次查看
wanghairun
Contributor I

Hi,

I try to generate a sd binary for imx8mm by yocto. So, I type the command below one by one. But it result in the failures. Could anyone help me on this problem?

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b  imx-linux-rocko -m imx-4.9.88-2.1.0-8mm_alpha.xml

repo sync

DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source ./fsl-setup-release.sh -b build.imx8mmevk

bitbake fsl-image-qt5

Loading cache: 100% |##############################################################################################################################################| Time: 0:00:00
Loaded 3287 entries from dependency cache.
Parsing recipes: 100% |############################################################################################################################################| Time: 0:00:02
Parsing of 2440 .bb files complete (2438 cached, 2 parsed). 3289 targets, 259 skipped, 9 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'weston-xwayland' (but /Projects/m845s/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'weston-xwayland' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['weston-xwayland']
ERROR: Required build target 'fsl-image-qt5' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-qt5', 'weston-xwayland']

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

@

Best Regards,

Hairun

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

2,422 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hairun

prereleases bsps are described on link
Alpha / Beta BSPs for Microprocessors|NXP 
and from attached Release Notes there is no qt support, also alpha prereleases may not
built properly as they are alpha (not fully tested) releases.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复