Ethernet compliance testing of Linux board based on iMX6UL & KSZ8041NLI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet compliance testing of Linux board based on iMX6UL & KSZ8041NLI

1,683 Views
ghanshyamdudhat
Contributor I

Dear Sir,

We are testing our product for Ethernet compliance testing through DSO Pre-compliance test module but as per test procedure need a test firmware with predefined test packet,

refer the required format -  scrambled, MLT-3 encoded /I/ code-groups (this is a 3-level pseudo-random bit sequence).

Can any one help us to create test application or share with us the application note or test firmware (Linux operating System) to perform the mentioned test.

 

Refer the below NXP and Mirochip PHY part details –

NXP Processer: iMX6UL

Ethernet PHY : KSZ8041NLI-TR

 

 Ethernet section schematic :

 

Labels (1)
0 Kudos
Reply
1 Reply

1,561 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ghanshyam 

I am afraid such ethernet compliance test application is not available, in general
one can aply to Professional Services to develop such test.
NXP Professional Services|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply