Yes, that's the exact guide I am following, I downloaded the docs package from that link and am using the pdf titled "Android_Quick_Start_Guide.pdf".
I'm not sure what you mean by the emmc images, I am using the "mfgtool2-android-mx6qp-sabresd-emmc.vbs" script to run MFGTool if that is what you are talking about. The image bundle came from this download: https://www.nxp.com/webapp/Download?colCode=IMX_O8.0.0_1.0.0_ANDROID_DEMO_SD&appType=license&Parent_...
And was named:
"android_O8.0.0_1.0.0_image_6dqpsabresd"
From that package I copied the following files and pasted them into the
Profiles\Linux\OS Firmware\files\android\sabersd folder for the MFGTool:
- boot-imx6qp.img
- partition-table.img
- recovery-imx6qp.img
- system.img
- u-boot-imx6qp.imx
- vendor.img
The partition-table.img was the one that came named that from the package, I believe it is for 8 Gigabyte storage.
Some other information that may or may not be relevant:
- The unit arrived with android already set up on an SD card. The card worked fine and boot up to android properly the first day. The next day it could not get past uboot. I don't know the cause but we did turn it on and off a number of times during the first day and may have switched it off during an inopportune time.
- As the guide instructed: SW6, the physical boot switch, is set to 00001100 (5 and 6 up, the rest down).
- By repeatedly starting and stopping the MFGTool after failure I did manage to get it to a "done" state once. However after configuring uboot for HDMI and running the system I only got a black screen with a non intractable cursor and an endlessly scrolling debug console.
- I notice I am getting a warning about mismatched CRCs in my debug console, which could be causing my problem.
I could not figure out how to add files to a reply and they were quite long so I added the MFGTool log and the debug console output to the original post.
Thanks,
Kelton