Error building wifi module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error building wifi module

1,741件の閲覧回数
rizwan_s
Contributor II

Hi Everyone,

I am working on wifi module for imx.6q nxp processor for android lollipop.

when i build the driver for wifi module, it shows the below error

receive.c:17:19: fatal error: stdio.h: No such file or directory
compilation terminated.

I am using arm cross compiler 4.6

Please suggest me, where am going wrong.

Regards

Rizwan Syed

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,630件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello rizwan,

    It is too less information you submitted about your WIFI module, so it is very hard to give you corresponding advice for your question, but generally speaking, for compiling WIFI driver, steps are like below:

------Compiling it independently to be a module( .ko)

Copy WIFI driver's source code to a directory.

------Modifying Makefile of the driver.

(1) Modifying Cross Compiler path

(2) Modifying Linux kernel path

(3) run make command

If you have done it by using above similar steps, and met issue you said, you can check if there exists the file in source code.

Hope above information can help you!

Best Regards,

Weidong

0 件の賞賛
返信

1,630件の閲覧回数
rizwan_s
Contributor II

Hi Weidong,

When am compiling the redpine wifi module independently , am getting the above error.

Thanks and Regards

Rizwan Syed

0 件の賞賛
返信