Enabling secure boot in the i.MX6 ULL 14x14 EVK board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling secure boot in the i.MX6 ULL 14x14 EVK board

ソリューションへジャンプ
1,206件の閲覧回数
Tamil751
Contributor I

Hi,

Is there any documentation available for enabling secure boot in the i.MX6 ULL processor. I can't find any docs. Also if you have an idea of how to implement this, please share it.

タグ(2)
0 件の賞賛
返信
1 解決策
1,187件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Tamil751,

I have included below the links one can refer to enable secure boot on i.MX6ULL,

 

I hope it helps!

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

Best Regards,
Dhruvit.

元の投稿で解決策を見る

3 返答(返信)
1,173件の閲覧回数
Tamil751
Contributor I

Hi @Dhruvit ,

Thanks for the reply. I'll explore these links. The last link asks for NXP Salesperson/FAE Name and Email. What do I have to give?

0 件の賞賛
返信
1,161件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport
You can connect with your NXP salesperson for more details regarding the same.

Thanks & Regards,
Dhruvit.
0 件の賞賛
返信
1,188件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Tamil751,

I have included below the links one can refer to enable secure boot on i.MX6ULL,

 

I hope it helps!

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

Best Regards,
Dhruvit.