Enabling secure boot in the i.MX6 ULL 14x14 EVK board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Enabling secure boot in the i.MX6 ULL 14x14 EVK board

跳至解决方案
1,201 次查看
Tamil751
Contributor I

Hi,

Is there any documentation available for enabling secure boot in the i.MX6 ULL processor. I can't find any docs. Also if you have an idea of how to implement this, please share it.

标记 (2)
0 项奖励
回复
1 解答
1,182 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Tamil751,

I have included below the links one can refer to enable secure boot on i.MX6ULL,

 

I hope it helps!

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

Best Regards,
Dhruvit.

在原帖中查看解决方案

3 回复数
1,168 次查看
Tamil751
Contributor I

Hi @Dhruvit ,

Thanks for the reply. I'll explore these links. The last link asks for NXP Salesperson/FAE Name and Email. What do I have to give?

0 项奖励
回复
1,156 次查看
Dhruvit
NXP TechSupport
NXP TechSupport
You can connect with your NXP salesperson for more details regarding the same.

Thanks & Regards,
Dhruvit.
0 项奖励
回复
1,183 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Tamil751,

I have included below the links one can refer to enable secure boot on i.MX6ULL,

 

I hope it helps!

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

Best Regards,
Dhruvit.