Enabling CAAM support for secure booting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling CAAM support for secure booting

3,560 Views
Deepu
Contributor III

Hi Freescale team,

I have to implement the support for CAAM module in linux kernel for Imx6 board to do the authentication of uImage. When I checked the kernel source code(linux-3.0.35) , I found some RNG self tests feature for CAAM hardware . How can we test this ?. Can anyone suggest what all things I have to take into account while doing this for both kernel and u-boot source.

Thanks in advance for your support .

0 Kudos
Reply
4 Replies

2,237 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply

2,237 Views
Deepu
Contributor III

hello Yuri,

I am using HAB  in imx6 with the secure hardwares like CAAM and SNVS. As a part of that in u-boot,we have to create  hab_caam_clock_enable and  hab_caam_clock_disable to make  secure hardwares to work.(I think its only for u-boot.

Kernel also has CAAM driver .My question is  what  is the purpose of this CAAM hardware and how will we check its working?

0 Kudos
Reply

2,237 Views
YixingKong
Senior Contributor IV

James, we would close the DI if no response in 3 days.

Thanks,

Yixing

0 Kudos
Reply

2,237 Views
yossishukron
Contributor III

hello James

are you asking about the verification for the Random Number Generator ?

are working in close mode ?

0 Kudos
Reply