IMX6 ,secure booting using HAB for kernel image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 ,secure booting using HAB for kernel image

9,005 Views
Deepu
Contributor III

Hi Freescale Support Team,

1.In Imx6 series processors,in order to make HAB to authenticate boot image (for eg: u-boot),we need to call HAB APIs from u-boot directly?.

2.How can I extend this secure booting feature for kernel Image?...For kernel image authentication also ,can i follow the same steps used for  signing the u-boot using CST tools .?.

3.Where should I include the authentation APIs in kernel to make HAB to authenticate the uImage?

4 Replies

3,766 Views
Yuri
NXP Employee
NXP Employee

The following are information sources :

“i.MX 6 Linux High Assurance Boot (HAB) User's Guide”

from Linux documentation.

https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_LINUXDOCS_BUNDLE&location=null

AN4581

“Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4”

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf

i.MX Trust Architecture presentation :

https://community.freescale.com/servlet/JiveServlet/download/313957-255581/20-i.MX_TrustArchitecture...

1.

The recent document states, that HAB API may be called from:

- Boot ROM.

− Other boot stages.

−APIs used in U-Boot in this session are:

hab_status_t(*report_event)(hab_status_tstatus, uint32_t index, uint8_t *event, size_t*bytes)

hab_status_t(*report_status)(hab_config_t*config, hab_state_t*state)

2.

Kernel image may be checked by U-boot, as mentioned in “i.MX 6 Linux High Assurance Boot (HAB) User's Guide” :

“The second stage is the authentication of uImage by U-Boot. authenticate_image is called

by U-boot to verify uImage when executing bootm.”

3,765 Views
satyadamarla
Contributor III

Hello Yuri,

authenticate_image, can this also be done for zImage?

Cheers,

Satya

0 Kudos
Reply

3,766 Views
Yuri
NXP Employee
NXP Employee

Hello,

> authenticate_image, can this also be done for zImage?

Yes.

Regards,

Yuri.

3,765 Views
Deepu
Contributor III

Hi  Yuri ,

     Thanks a lot for your post .I have all documents except i.MX 6 Linux High Assurance Boot (HAB) User's Guide .This document is very helpfull .Thanks for your help.

0 Kudos
Reply