Enable VLPR mode IMX8DXL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable VLPR mode IMX8DXL

Jump to solution
3,612 Views
bsourav47
Contributor II

Hello Team,

We are using iMX8DQX processor and we would like to enable the VLPR mode. We have already understood and done the VLLS mode, but we would like to enable the VLPR mode.

We checked and understood that the clock will be reduced to 24Mz. Do we need to put the peripherals to 

SC_PM_PW_MODE_LP prior going to VLPR ?
Can you please guide the steps that we need to do for VLPR ? 
 
Regards,
Sourav
0 Kudos
Reply
1 Solution
3,374 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi @bsourav47,

Please create a support ticket, there is sensitive information that can be sent over a ticket. The ticket may be assigned to me.

Regards!

View solution in original post

0 Kudos
Reply
10 Replies
3,565 Views
bsourav47
Contributor II

Dear @JosephAtNXP ,

Could you please respond to the queries.

Regards,

Sourav

0 Kudos
Reply
3,593 Views
bsourav47
Contributor II

Hello @JosephAtNXP ,

Thanks for responding. I have downloaded the same and saw that only the UART was put to off state. Any other peripherals are not.

I have the following questions:

  • Will I need to explicitly put the peripherals to SC_PM_PW_MODE_LP  or SC_PM_PW_MODE_OFF prior to VLPR mode ?
  • Will I be able to read ADC in VLPR mode ? As the clock will change to 24MHz will I need to re-initialize ADC ?
  • How will the system wake up from VLPR mode to RUN mode ? Is VLPR similar to KS1 ?

Regards,

Sourav

0 Kudos
Reply
3,547 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi @bsourav47,

Actually the experts advise using VLLS:

"Current reduction under VLPR mode is little. So when customers wants to reduce the current, it is a better choice to enter other mode such as VLLS"

Regards

0 Kudos
Reply
3,540 Views
bsourav47
Contributor II

Hello @JosephAtNXP ,

I totally get your point, but for a particular use case we are investigating the VLPR mode and would kindly request your support on that please.

If you could please respond to the queries that I posted above.

Additionally we would also want to know if we can detect button press in VLPR mode.

Regards,

Sourav

0 Kudos
Reply
3,431 Views
bsourav47
Contributor II

Hello @JosephAtNXP ,

Any update from your side please ?

 

Regards,

Sourav

3,391 Views
bsourav47
Contributor II

Hello @JosephAtNXP ,

Please let me know the answer to the queries?

Regards,

Sourav

0 Kudos
Reply
3,385 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi @bsourav47,

Please review your email.

Regards

0 Kudos
Reply
3,380 Views
bsourav47
Contributor II

Hello @JosephAtNXP ,

I do not understand when you say please review your email.

You mentioned this : Actually the experts advise using VLLS: "Current reduction under VLPR mode is little. So when customers wants to reduce the current, it is a better choice to enter other mode such as VLLS" 

To which I responded as : "I totally get your point, but for a particular use case we are investigating the VLPR mode and would kindly request your support on that please. If you could please respond to the queries that I posted above. Additionally we would also want to know if we can detect button press in VLPR mode."

So I am not sure what I should review in the email. Please clarify. I would still require to know the following for the VLPR mode, this is an investigation the Suzuki team is doing.

  • Will I need to explicitly put the peripherals to SC_PM_PW_MODE_LP  or SC_PM_PW_MODE_OFF prior to VLPR mode ?
  • Will I be able to read ADC in VLPR mode ?
  • As the clock will change to 24MHz will I need to re-initialize ADC ?

I read all my emails and posts. So if could kindly respond then it will be of great help. I still do not have any clear reply from NXP, only you suggested VLLS mode which we already have in our product. Please note we are investigating VLPR mode for a particular use case

Regards,

Sourav

0 Kudos
Reply
3,375 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi @bsourav47,

Please create a support ticket, there is sensitive information that can be sent over a ticket. The ticket may be assigned to me.

Regards!

0 Kudos
Reply
3,595 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

To switch power modes, there is a Cortex-M demo app that allows power switching the cores, please build the SDK for 8DXL and build demo_apps/power mode switch demo.

MCUX

Regards

0 Kudos
Reply