iMx8-m | control regulator gpio from user space

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMx8-m | control regulator gpio from user space

Jump to solution
566 Views
Harshkumar_Patel
Contributor I

Hello Team,

Trying to control regulator pin (gpiochip3-25) from user space on i.MX 8 with kerel 5.10.0-30-amd64 but it is not allowing to change.

echo enabled > /sys/devices/platform/regulator-lte-on/regulator/regulator.4/state
sh: /sys/devices/platform/regulator-lte-on/regulator/regulator.4/state: Permission denied

Additionally, It is using generic regulator driver "regulator-fixed" and  "CONFIG_REGULATOR_USERSPACE_CONSUMER" kernel config is enabled but still same.

Further there is one doc regulator userspace-consumer - NXP Community which describes to do this with different driver and specific device tree changes.

Question:
Is there any better way to control regulator pin state without following the steps mentioned in above link especially getting special dts changes?

Thanks in advance.

regards,
Patel

0 Kudos
Reply
1 Solution
429 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Harshkumar_Patel!

Thanks for confirming the GPIO toggle using the gpio-led driver.

 

Since gpiochip3-25 controls modem power and must remain ON, I recommend using regulator-fixed. It offers better integration with the power management framework and ensures stability during suspend/resume, kernel stalls, or high system load. The gpio-led driver may not reliably maintain the GPIO state in those scenarios.

 

However, if maintaining the power rail only during active mode is sufficient, the gpio-led driver can be used with a pull-up resistor to keep the signal HIGH, and the rail can be turned off when no longer needed.

 

Best regards,
Chavira

View solution in original post

0 Kudos
Reply
5 Replies
403 Views
Harshkumar_Patel
Contributor I

Hi Chavira,

Thanks for the quick and clear response.

Further, in case you are aware,
As controlling regulator from user space is most common need, is there plan to have userspace_regulator patch to be part of next revision of i.MX8 yocto SDK?

Thanks

0 Kudos
Reply
356 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Harshkumar_Patel!

Unfortunately, we do not have plans to provide a patch, as we are not responsible for developing the driver in question.

 

Please note that all resources shared in the community are intended for reference purposes only. Officially supported software from NXP is available on GitHub, and we typically provide manuals to guide users on how to use it in each specific case.

 

Best regards,
Chavira

0 Kudos
Reply
533 Views
Harshkumar_Patel
Contributor I

Hi Chavira,

Thank you for super-fast and clear response.
I verified expected gpio toggle using the gpio-led driver but want expert opinion before using this option.

As you may noticed that we are using gpiochi3-25 for enabling modem power and it must remain ON.
Using it as "gpio-led" instead of "regulator-fixed", do you see any issue in case of kernel stall or overloading or latency or low-power-modes?

Thanks




0 Kudos
Reply
430 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Harshkumar_Patel!

Thanks for confirming the GPIO toggle using the gpio-led driver.

 

Since gpiochip3-25 controls modem power and must remain ON, I recommend using regulator-fixed. It offers better integration with the power management framework and ensures stability during suspend/resume, kernel stalls, or high system load. The gpio-led driver may not reliably maintain the GPIO state in those scenarios.

 

However, if maintaining the power rail only during active mode is sufficient, the gpio-led driver can be used with a pull-up resistor to keep the signal HIGH, and the rail can be turned off when no longer needed.

 

Best regards,
Chavira

0 Kudos
Reply
548 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Harshkumar_Patel,

By default, the regulator-fixed driver does not allow direct control from user space. To enable this functionality, you would typically need to modify the driver or adjust the device tree to include a regulator-userspace-consumer node.

However, a simpler and more flexible alternative is to declare the regulator's enable GPIO using the gpio-led driver. This approach allows you to control the GPIO directly from user space using standard interfaces like sysfs or libgpiod, without needing to modify the regulator framework or device tree extensively.

This method is especially useful when you only need basic on/off control and want to avoid deeper kernel or DTS changes.

Best regards,
Chavira

0 Kudos
Reply