Enable Phonegap framework and java for IMX6q using LTIB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable Phonegap framework and java for IMX6q using LTIB

1,622件の閲覧回数
shalinikp
Contributor II

Is it possible to enable phonegap and java on LTIB for imx6q.  Please reply if any one has enabled it.

ラベル(2)
0 件の賞賛
返信
1 返信

1,503件の閲覧回数
b36401
NXP Employee
NXP Employee

Java virtual machines are able to run on the MX6x BSPs. However we do not offer any java VM in the BSP.

Oracle has pre-built versions of Java Virtual Machine for ARM Processors. It's possible to download them here:

http://www.oracle.com/technetwork/java/embedded/embedded-se/downloads/index.html

You can find mode details in this document:

https://community.freescale.com/docs/DOC-1478

0 件の賞賛
返信