Effect of i.MX5x Linux BSP patch.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Effect of i.MX5x Linux BSP patch.

Jump to solution
1,013 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX5x Linux BSP (L2.6.35_xx).

Our partner found the following patch, and they want to know the effect of the patch.

linux-2.6-imx.git - Freescale i.MX Linux Tree

I checked the patch, and understood the patch changes L1 cache line size.

So I think there is no bad effect by the patch and improve data transfer efficiency.

Is my understanding correct?

Best Regards,

Satoshi Shimoda

Labels (3)
0 Kudos
Reply
1 Solution
925 Views
Yuri
NXP Employee
NXP Employee

Hello,

   
  Your understanding is correct.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
926 Views
Yuri
NXP Employee
NXP Employee

Hello,

   
  Your understanding is correct.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply