Effect of i.MX5x Linux BSP patch.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Effect of i.MX5x Linux BSP patch.

ソリューションへジャンプ
1,766件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX5x Linux BSP (L2.6.35_xx).

Our partner found the following patch, and they want to know the effect of the patch.

linux-2.6-imx.git - Freescale i.MX Linux Tree

I checked the patch, and understood the patch changes L1 cache line size.

So I think there is no bad effect by the patch and improve data transfer efficiency.

Is my understanding correct?

Best Regards,

Satoshi Shimoda

ラベル(3)
0 件の賞賛
返信
1 解決策
1,678件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   
  Your understanding is correct.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,679件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   
  Your understanding is correct.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信