Eample using the GPU2D to overlay video stream before encoding via OpenGL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Eample using the GPU2D to overlay video stream before encoding via OpenGL?

1,928件の閲覧回数
Larry5335
Contributor IV

I am looking for a method to do an accelerated, color keyed, blit onto a frame buffer prior to sending it to the video encoder.  We would use this to composite a graphic overlay onto the video stream.  I’ve read  http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf but I would need the IPU to deposit the result back into memory to be encoded instead of rendering it to an output.  Do you have an example using the GPU2D to do this via OpenGL?

ラベル(6)
タグ(2)
0 件の賞賛
返信
1 返信

1,501件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Please take a look at the IMX6_GPU_SDK, it includes sample codes and GPU2D similar that the one you are looking for:

i.MX6Q: i.MX 6Quad Processors – Quad Core

Regards


Have a great day,

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信