Eample using the GPU2D to overlay video stream before encoding via OpenGL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eample using the GPU2D to overlay video stream before encoding via OpenGL?

1,945 Views
Larry5335
Contributor IV

I am looking for a method to do an accelerated, color keyed, blit onto a frame buffer prior to sending it to the video encoder.  We would use this to composite a graphic overlay onto the video stream.  I’ve read  http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf but I would need the IPU to deposit the result back into memory to be encoded instead of rendering it to an output.  Do you have an example using the GPU2D to do this via OpenGL?

Tags (2)
0 Kudos
Reply
1 Reply

1,518 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Please take a look at the IMX6_GPU_SDK, it includes sample codes and GPU2D similar that the one you are looking for:

i.MX6Q: i.MX 6Quad Processors – Quad Core

Regards


Have a great day,

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply