EMMC BOOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMMC BOOT

Jump to solution
3,522 Views
jeffery
Contributor III

Now we are developing android 8.0.0 using imx6q board,and is successful to build the android image.

But  usiing mfgtools to download images,it appear to " Jumping to OS image. "

Because we use emmc boot ,so I think we should modify u-boot to emmc boot in android o source code,but it doesn't work.

How to modify to emmc boot?

thanks!

Labels (1)
0 Kudos
Reply
1 Solution
3,327 Views
igorpadykov
NXP Employee
NXP Employee

Hi 贻才 林 

such error happens when manufacturing firmware (files in mfg tools /firmware folder)

were not rebuilt for custom board. Steps are described in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide. Also had board passed ddr testi.MX6/7 DDR Stress Test Tool V2.90 

and boot linux. New calibration coefficients found from test should be put in uboot/board/..mx6sabresd

/mx6q_4x_mt41j128.cfg file and image should be rebuilt.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
3,328 Views
igorpadykov
NXP Employee
NXP Employee

Hi 贻才 林 

such error happens when manufacturing firmware (files in mfg tools /firmware folder)

were not rebuilt for custom board. Steps are described in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide. Also had board passed ddr testi.MX6/7 DDR Stress Test Tool V2.90 

and boot linux. New calibration coefficients found from test should be put in uboot/board/..mx6sabresd

/mx6q_4x_mt41j128.cfg file and image should be rebuilt.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------