EMMC BOOT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,529件の閲覧回数
jeffery
Contributor III

Now we are developing android 8.0.0 using imx6q board,and is successful to build the android image.

But  usiing mfgtools to download images,it appear to " Jumping to OS image. "

Because we use emmc boot ,so I think we should modify u-boot to emmc boot in android o source code,but it doesn't work.

How to modify to emmc boot?

thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
3,334件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 贻才 林 

such error happens when manufacturing firmware (files in mfg tools /firmware folder)

were not rebuilt for custom board. Steps are described in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide. Also had board passed ddr testi.MX6/7 DDR Stress Test Tool V2.90 

and boot linux. New calibration coefficients found from test should be put in uboot/board/..mx6sabresd

/mx6q_4x_mt41j128.cfg file and image should be rebuilt.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
3,335件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 贻才 林 

such error happens when manufacturing firmware (files in mfg tools /firmware folder)

were not rebuilt for custom board. Steps are described in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide. Also had board passed ddr testi.MX6/7 DDR Stress Test Tool V2.90 

and boot linux. New calibration coefficients found from test should be put in uboot/board/..mx6sabresd

/mx6q_4x_mt41j128.cfg file and image should be rebuilt.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------