EMMC BOOT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

EMMC BOOT

跳至解决方案
3,525 次查看
jeffery
Contributor III

Now we are developing android 8.0.0 using imx6q board,and is successful to build the android image.

But  usiing mfgtools to download images,it appear to " Jumping to OS image. "

Because we use emmc boot ,so I think we should modify u-boot to emmc boot in android o source code,but it doesn't work.

How to modify to emmc boot?

thanks!

标签 (1)
0 项奖励
回复
1 解答
3,330 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 贻才 林 

such error happens when manufacturing firmware (files in mfg tools /firmware folder)

were not rebuilt for custom board. Steps are described in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide. Also had board passed ddr testi.MX6/7 DDR Stress Test Tool V2.90 

and boot linux. New calibration coefficients found from test should be put in uboot/board/..mx6sabresd

/mx6q_4x_mt41j128.cfg file and image should be rebuilt.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
3,331 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 贻才 林 

such error happens when manufacturing firmware (files in mfg tools /firmware folder)

were not rebuilt for custom board. Steps are described in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide. Also had board passed ddr testi.MX6/7 DDR Stress Test Tool V2.90 

and boot linux. New calibration coefficients found from test should be put in uboot/board/..mx6sabresd

/mx6q_4x_mt41j128.cfg file and image should be rebuilt.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------