EIM Burst Synchronous Mode in Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM Burst Synchronous Mode in Linux

ソリューションへジャンプ
1,772件の閲覧回数
jzabalza
Contributor II

Hello

Has anyone used the WEIM Burst Synchronous Mode in Linux?

Some example?

Thanks.

1 解決策
1,676件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jose

burst mode can be configured using CSxGCRx EIM registers, in linux dts this is

the timing array "weim-cs-timing"

imx-weim.txt\bus\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

EIM is supported in i.MX6Q Sabre AI board

imx6q-sabreauto-gpmi-weim.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,677件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jose

burst mode can be configured using CSxGCRx EIM registers, in linux dts this is

the timing array "weim-cs-timing"

imx-weim.txt\bus\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

EIM is supported in i.MX6Q Sabre AI board

imx6q-sabreauto-gpmi-weim.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信